12/11/2024 1:04 AM | |
Joined: 3/21/2015 Last visit: 8/22/2025 Posts: 60 Rating:
|
Hello Experts, I also have a similar issue, I am using PCS7 9., i have no faults during my compilation of the OS and if I do small changes or even no changes and try to download it, the system will not allow me to do "only changes" download but the entire system, but I stop the server is always a thing no one likes to do. Is there any solution for this "problem"? Important to mention have a redundant server running here. Thank you in advance. Nick. ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 12/11/2024 09:01:38New subject after splitting |
|
12/11/2024 10:34 AM | |
Joined: 3/14/2008 Last visit: 9/11/2025 Posts: 2216 Rating:
|
Hi, Please check the following manual, chapter 19 page page 311. Check if you fulfill the requirements, some changes cannot be done with OS download change (chapter 19.8). Another usefull manual is the Compendium part A Configuration guidelines. Chapter 11 describes OS downloading changes, see chapter 11, page 395. |
Last edited by: Oreca at: 12/11/2024 10:35:50If I could help you, you can use the RATE button. Thank you. |
|
12/12/2024 1:08 PM | |
Joined: 3/14/2008 Last visit: 9/11/2025 Posts: 2216 Rating:
|
Hi, No problem!, In Simatic Manager, go to your OS server project and right click on the OS station of the master server and select: Display load log. Hopefully something interesting is shown there. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on