9/15/2025 1:33 AM | |
Joined: 9/15/2025 Last visit: 9/15/2025 Posts: 3 Rating:
|
我已购买 SIMIT 11.3 软件的正版许可证,现在需要使用 SIMIT 连接 KUKA 机器人。我观看了 SIMIT 连接 KUKA Offcelite 软件的演示视频,但我的 SIMIT 缺少“KUKA 连接器”。
|
9/15/2025 9:30 AM | |
Joined: 9/15/2025 Last visit: 9/15/2025 Posts: 3 Rating:
|
Dear Expert, I am in urgent need of this assistance and am deeply grateful. |
9/15/2025 1:06 PM | |
Joined: 2/1/2010 Last visit: 9/16/2025 Posts: 213 Rating:
|
If you look on the link below under robot connections there is a guide definition and instructions to open a SIOS ticket for application examples. SIMIT Couplings, applicative expansions of the interface Chapter 4 is Kuka. Based on how the diagram is shown, it appears that its SHM connection (Shared Memory). I haven't connected Kuka to SIMIT yet so I can't confirm for sure, but you can research Share Memory Coupling in PUD and how to connect that to OffliceLite Y200 should be evident if it does have the SHM connector on Kuka side. You may be able to get the application example which includes Kuka from SIOS ticket confirming (or not) the above. |
If my post helped you, please rate. Thanks. |
|
This contribution was helpful to
1 thankful Users |
Follow us on