3/13/2025 6:08 AM | |
Joined: 5/20/2020 Last visit: 5/21/2025 Posts: 5 Rating:
|
We have PCS7 7.1 with Simatic manager every time when i tried to configure the station it configures successfully and the station is online in the Batch server station configuration editor. But when trying to download after configuration, the batch application standby cannot be downloaded. I tried many times by Set PG/PC is set to Local Internal or to the Terminal bus. Please find the screenshots and help me to resolve this issue. Engineering station is DOWNES08 and Batch standby server is DOWNBA02. AttachmentBatch application download issue.zip (222 Downloads) |
3/13/2025 8:37 AM | |
Joined: 3/14/2008 Last visit: 9/16/2025 Posts: 2216 Rating:
|
Hi, Make sure the configuration of the project is downloaded to your ES station first so that "he" knows all the addresses and such. Make sure every project inside the MP is save and compiled. Furthermore, the batch server normally has no connection with the plant bus. You could do this to enable AS configured batch, but maybe this is the problem because the PC cannot be reached via terminal bus. Another way to accomplish this is to import the station configuration via option: "Import Station" in the station configuration editor. The configuration is saved on the ES and you can load that file directly to the batch server. It's in format .XDB.
|
If I could help you, you can use the RATE button. Thank you. |
|
4/1/2025 7:26 AM | |
Joined: 1/11/2019 Last visit: 8/14/2025 Posts: 899 Rating:
|
Check for the windows update |
4/2/2025 6:59 AM | |
Joined: 5/20/2020 Last visit: 5/21/2025 Posts: 5 Rating:
|
Running the application on Windows Server 2003 R2 SP2 |
Follow us on