1/4/2019 9:36 AM | |
Joined: 9/9/2015 Last visit: 5/28/2024 Posts: 727 Rating: (270) |
Dear Ad_181......., Can you press the module driver "Tab" to see more details error log? Attached with screenshot. And then , you might need to update your driver to latest one. copy all the blocks from the latest version library, update the block type. Look for library, 7.1 SP3 Up4. If possible, update the rest to latest one as well. Hope it helps. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
1/7/2019 7:17 AM | |
Joined: 9/9/2015 Last visit: 5/28/2024 Posts: 727 Rating: (270) |
Dear Ad_181.., It should be resolved when you use the correct version of CH_AI. 1. Check your installed software library. Search - Software -> look for Inst. Software. 2. Check your SIMATIC PCS 7 Library version V71 SP3 Upd4 3. Open Project-> Libraries-> PCS 7 Library V71. -> Copy all the blocks from the library to your project block folder. 4. Open CFC editor, Option-> Block Type 5. Select all from the offline block folder to insert into chart folder. 6. Full Compile again Hope it helps. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to1 thankful Users |
1/9/2019 2:15 AM | |
Joined: 9/9/2015 Last visit: 5/28/2024 Posts: 727 Rating: (270) |
Dear Ad_181.., Welcome. You may click the Action and Mark resolved. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to1 thankful Users |
Follow us on