4/22/2021 6:07 PM | |
Joined: 3/19/2019 Last visit: 7/17/2024 Posts: 97 Rating:
|
I have another doubt on tp1500 HMI. In our project we have 135 Analog Inputs, 32 Valves and 43 pumps. nearly 200 instruments. And we decided to use faceplate option for these all instruments, On that faceplate customer want one confirm button option for execute the operation. for example if operator wants to change the valve mode from manual to auto, then 1st he have to select the auto after that he press confirm button so that only the valve go to auto mode. this confirmation need for every button and set points like auto/manual, start/stop, open/close, alarm set point. so anyone can give me best solution for this case as soon as possible. and i had attached screen shots of that faceplate, the confirm button represented as 'exec'. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/23/2021 08:15:20New subject after splitting "If you want the answer - ask the question" |
|
Follow us on