12/7/2023 11:39 AM | |
Joined: 12/7/2023 Last visit: 12/19/2023 Posts: 3 Rating: (0) |
Dear Team, I am also facing the same issue on S71500 CPU 1515-2PN (6ES7515-2AM01-0AB0) is that CPU installed in our plant around two years and working well but suddenly CPU went to STOP mode and all communication goes down and after reset the PLC POWER OFF and turns to ON it becomes normal (RUN) mode but after few days CPU again went to STOP mode and after Power reset than it moves to Connecting mode... And now it was not going to RUN mode even power Reset , Please guide us what is the root cause of CPU failure. ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 12/07/2023 12:29:59New subject after splitting |
|
12/7/2023 12:32 PM | |
Joined: 6/19/2019 Last visit: 10/10/2024 Posts: 700 Rating: (74) |
Go online and diagnostic and see what is the problem why CPU go to STOP mode |
12/12/2023 5:04 AM | |
Joined: 12/7/2023 Last visit: 12/19/2023 Posts: 3 Rating: (0) |
When i get online with PC/PG interface it shows stop mode |
Follow us on