3/24/2018 1:19 PM | |
Posts: 11 Rating: (0) |
HELLO, THE FAILURE IS: # 120008 OPERATOR UNITS SWICHOVER, PLC TIMEOUT: 1010 THIS IS IN THE HMI, THE RED LED IS: SF = LIGHTS UP WHENEVER DRIVE ERRORS OCCUR. GOES OUT AFTER THE SYSTEM IS BOOTED IN ERROR-FREE CONDITION. I THINK THAT THE PROGRAM WAS EXTRACTED, BEFORE ALL THE LEDS WERE LITTLE ON, WHAT I PERFORMED WAS THE FOLLOWING PROCEDURE: OFF, - S3> 1, S4> 3 ON - LED "6" APPEAR - THEN CONFIGURE S3> 0, THEN S4> 2> 3> 2, S4> 0, THEN LED "6" PLUS -5V, MORE SF "LED RED". TAKE IT AS A REFERNCIA FROM THIS PLACE. NOW I NEED TO START THE SYSTEM. THANK YOU VERY MUCH FOR YOUR HELP Attachment120008.docx (53 Downloads) |
Follow us on