12/10/2020 3:25 PM | |
Joined: 11/5/2020 Last visit: 8/8/2024 Posts: 1 Rating: (0) |
How to connect mag 5000 to measure flow and volume to calibrate another meters with high accuracy what is the PLC type and modules numbers I HAVE 17 DI 15 DO AI (temperature 0-100 c &pressure max 25 bar & flow meter (measuring flow and volume of water) & AO (SPEED OF WATER PUMP(AC DRIVER)) THE SYSTEM CONNECTED TO PC . The hard ware of PLC and the best connection way between the flowmeter (Siemens mag5000 ) and the plc . ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 12/11/2020 15:17:52New subject after splitting |
|
Follow us on