Industry Online Support
Technical Forum
8/27/2012 11:38 AM | |
Posts: 3 Rating: (0) |
Hi All I'm having a issue regard to MM 440 that sometime frequency of MM440 reduce to minimum Hz (5Hz) and then increase to Hz's working, therefore speed of motor reduce also. and input signal are 0~10V which suppied by output isolator card. So, I sent a file attached of trend speed of motor for more detailer Please give me someguides and hepl me to solve that issue And please let me know if you need to info more Thanks D.Tuan Attachmentimg-827160155.pdf (525 Downloads) |
9/1/2012 7:54 AM | |
Posts: 3 Rating: (0) |
Thanks, I will check agian !! |
Follow us on