Industry Online Support
Technical Forum
7/28/2009 11:46 AM | |
Posts: 13 Rating: (0) |
I have: type: switch with graphic |
7/28/2009 1:34 PM | |
Posts: 13 Rating: (0) |
On WinCC 6.2 in object palette exists option Check Box....but what should I put in WinCC flexible 2008? |
7/28/2009 3:11 PM | |
Posts: 8946 Rating: (999) |
Hmmm... can you upload your project? |
7/29/2009 3:31 PM | |
Joined: 5/8/2006 Last visit: 4/29/2024 Posts: 1085 Rating: (77) |
Hi If you use a switch with a graphic which looks like a check box, then you can connect a tag to this switch. If you use internal tags, then the tags lose thecurrent valueafter the shutdown of the Runtime. You have two possibilities to get the value ofa tag after a shutdown of the Runtime: 1. You can save the value of the tags in an file (only with a panel as from 270 series). -> Link tothe FAQ for panels! -> Link to the FAQ for PCs! 2. You can use PowerTags whichare stored ina PLC. Bye |
Follow us on