2/2/2024 10:07 PM | |
Joined: 3/14/2008 Last visit: 6/25/2024 Posts: 2072 Rating: (929)
|
Hi, These signals are used when allocating EM by an EPH. You need to have a EPHT (Equipment Phase Type) and a EMT (Equipment Module Type). With this concept, you can use the same EM for different phases. In order to use the EM, you need to assign an allocation strategy like claim Now or claim by a delay time. In the SFC visualization you can view which EM has been allocated to which EPH via a new view in the faceplate. The CM also have those signals, but in v9.0 they are "reserved" for future use. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on