3/29/2021 8:45 AM | |
Joined: 6/4/2010 Last visit: 9/30/2024 Posts: 387 Rating:
|
Dear forum member, I have heard of similar cases. There is the patch PCR_1080835_Flex_Client_4.2.0116.0 to address such an issue. You can find the patch under the link below: https://support.industry.siemens.com/cs/ww/en/view/109783457(access only via Internet or Extranet for Solution Partners). Please note that there may be a workaround. The behavior could also be corrected using “Anchor” position base to the symbol and the navigation link. Please note that I cannot confirm, if it really is the issue above, just based on the image provided. You may contact the local Customer Support and provide the project backup or remote access, in case the advice does not help. Best regards, Albis |
Follow us on