9/9/2025 2:54 AM | |
Joined: 3/31/2025 Last visit: 9/9/2025 Posts: 1 Rating:
|
can everyone help me with this when i simulate the wincc unified it still cannot run ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 09/09/2025 08:03:46New subject after splitting |
|
9/9/2025 1:23 PM | |
Joined: 8/3/2009 Last visit: 9/15/2025 Posts: 16409 Rating:
|
Hello xuan thinh_nguyen le check with https://localhost and also with https://[IPaddress] (use of course you IP address ;-) ) If there is also the same error as in your screenshot then the Unified Website does not run. Open the IIS (internet Information server) and check if the Unified Website is installed at the Websites and also if it is Running state. If not then Check if you have installed the Unified PC RT and if you have set up the configuration: https://support.industry.siemens.com/cs/de/en/view/109806850 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on