6/5/2025 9:34 AM | |
Joined: 8/3/2009 Last visit: 9/12/2025 Posts: 16409 Rating:
|
Hello SerkanC2 usually in V20 you only have to start the simiulation. If you start this, the Runtime should appear and the "default User" should be automatically logged in. But if you wan to log in with anohter user you have to open the login dialog or use systemfunction for change user. You can try to open manually in the browser the landing page with only the own IP or name. Then the startscreen with the 4-5 Buttons should appear where you can start RT or open the User Management. What happens if you want to open the User management? You should also check if you have set up your Runtime/Simulation correctly: https://support.industry.siemens.com/cs/de/en/view/109806850 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on