12/23/2024 9:29 AM | |
Joined: 5/6/2022 Last visit: 9/15/2025 Posts: 589 Rating:
|
Hi AutoGen_8364008, Could you please specify exactly what procedure you are following and the exact model/reference of the panel you are using? These 'Mobile Panels' panels only have the image version up to V17 update 8, I don't understand which V18 panel images you indicate exactly that you have loaded in V19. I recommend you to check the following FAQ where you can find the panel images and more information: In your case, if you are using TIA Portal version V19, you have to load the panel images from V17 to be able to load into the panel for the 'Mobile Panels' there is no V18 image version. Make sure that in the address "C:\Program Files "Automation Portal V19" the images of the V17 version are loaded.
|
If this Information really helps, you could use the Rate function |
|
1/9/2025 8:07 AM | |
Joined: 8/3/2009 Last visit: 9/16/2025 Posts: 16436 Rating:
|
Hello AutoGen_8364008 The best way would be to check if you have set the Panel device Version in your TIA project to the latest available V17.0.0.0 Then use the PIU Updater to install the latest available Panel Image to your TIA V19: https://support.industry.siemens.com/cs/de/en/view/109825750 If the PIU Updater does not work (there are a few issues at the moment regarding the Login), you can use the way with the offline download like explained in documentation of Chapter V1.2 in the FAQ above for offline installing the images to your V19 (the way of doing this is identical in every TIA Version) Then you should have all data and the transfer and OS Update should work. Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on