6/21/2021 2:23 PM | |
Joined: 12/12/2016 Last visit: 7/25/2025 Posts: 640 Rating:
|
Hello Ratan, May I ask which brand/model of WIFI Stick you are using? Most likely its an issue with incompatible drivers in Example Image V1.0.2, a new build from master branch could fix the issue as some improvements have been done. Alternatively you could also e.g install crontab and add this command to run dhclient @reboot. BR |
Last edited by: Fe_lipe at: 06/21/2021 14:23:55 |
|
6/21/2021 3:09 PM | |
Joined: 12/7/2010 Last visit: 7/28/2025 Posts: 94 Rating:
|
HELLO I AM USING Edimax EW-7811Un Model for wifi stick as you have suggested to do "Alternatively you could also e.g install crontab and add this command to run dhclient @reboot." but this problem also comes when internet goes off to on. |
6/24/2021 8:32 AM | |
Joined: 12/7/2010 Last visit: 7/28/2025 Posts: 94 Rating:
|
HELLO
|
6/24/2021 11:29 AM | |
Joined: 12/12/2016 Last visit: 7/25/2025 Posts: 640 Rating:
|
Hello Ratan, wicd-curses seems to work-around the buggy drivers by attempting a reconnect after the connection is dropped. Please check out the third answer on here. I have the same WIFI Stick and reconnect is working for me after enabling the "Automatically connect to this network" option. BR |
Last edited by: Fe_lipe at: 06/25/2021 12:57:05 |
|
Follow us on