1/13/2015 7:43 AM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2149)
|
Hello Anil Mali, what do you do with the licence-keys in a rar-archive. They are not delivered in a rar-archive on the USB-Stick. They have to be directly in the hidden folder "AX NF ZZ" on the USB-Stick, and when you transfer them to the harddrive via ALM, they are on the harddrive in the hidden folder "AX NF ZZ". You may have destroyed the licence-keys by compreesing them with RAR. For repairing them, you should contact the Authorization-Hotline http://support.automation.siemens.com/WW/view/en/772175 Regards Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
This contribution was helpful to1 thankful Users |
Follow us on