1/9/2015 7:45 AM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2146)
|
Hello Anil Mali, do you see the license-keys on the USB-Stick, only with the common Windows-Explorer, but not in the ALM ? If you can see them in the ALM, you can mark them with the mouse and draw them to the harddrive. If you can see them not in the ALM, they may be corrupt, an you should contact the Authorzation-Hotline. see: http://support.automation.siemens.com/WW/view/en/772175 Regards Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
1/9/2015 1:17 PM | |
Posts: 22 Rating: (1) |
Thank you sir... Ok When i connect to PC & see in ALM didnt show any license but when i copy in computer & archive it shows all license.
|
1/12/2015 5:15 PM | |
Posts: 22 Rating: (1) |
Dear Sir, Please find attach snap of ALM.
|
1/13/2015 6:16 AM | |
Posts: 22 Rating: (1) |
Dear Sir, Please find print screen for the same. In Simatic_1 print screen:- I copy "AX NF ZZ" file from USB stick dongle on my computer Drive. another print screen on next post Attachmentsimatic_1.jpg.pdf (169 Downloads) |
1/13/2015 6:17 AM | |
Posts: 22 Rating: (1) |
Attachmentsimatic_2.pdf (152 Downloads) |
Follow us on