4/24/2018 3:43 PM | |
Joined: 10/26/2011 Last visit: 4/22/2024 Posts: 760 Rating: (190)
|
If you have PCS 7 V8.2, you have to buy PDM V9.1. There are two types of deliveries possible: DVD package or online download. Both have a setup (exe file) inside. https://support.industry.siemens.com/cs/ww/en/view/109748101 |
Last edited by: Thunderstorm at: 4/24/2018 3:44:43 PMLast edited by: Thunderstorm at: 4/24/2018 3:45:19 PMSIMATIC PCS 7 - Overview |
|
This contribution was helpful to1 thankful Users |
4/24/2018 3:52 PM | |
Joined: 4/8/2016 Last visit: 2/13/2024 Posts: 133 Rating: (45) |
Hey kopo_vagyok, normally you use the PCS 7 setup.exe and just select the package e.g. PDM which you want to add. But this is not possible for you because PCS 7 V8.2 has PDM V9.0 Upd1 on the DVD. If you have bought PDM V9.1 than you should have got a DVD or a download with the installation files for PDM V9.1. Please note that if you use PDM V9.1 in PCS 7 < V9.0, you need additionally SIMATIC Logon V1.6. You can find the information that SIMATIC Logon V1.6 must be purchased in this case additionally in the product note: https://support.industry.siemens.com/cs/ww/en/view/109748101 |
Kind regards |
|
This contribution was helpful to1 thankful Users |
4/25/2018 3:08 PM | |
Joined: 5/3/2017 Last visit: 4/19/2024 Posts: 673 Rating: (216) |
Hello kopo, the update for SIMATIC PDM V9.0 SP1 Update 3 isn't online. Not all updates published at the Industry Online Support. For example the update for SIMATIC PDM V9.0 SP1 Update 2 is online (SIMATIC PDM V9.0 SP1 Update 2). With regards |
This contribution was helpful to1 thankful Users |
Follow us on