4/20/2020 6:32 PM | |
Posts: 8 Rating: (0) |
Hi Mr.daniel. No sir. Absolutely we don't mind attach the diagnostic buffer or any further needed documents. Tha diagnostic buffer is in the attached files for this answer. Note_1: This text was upload just before fixing communication with ET200M IM.no.3 Note_2: The 2 ddresses in diagnostic buffer : 1. PIW 256 is for RFID reader which attached in the same rack with ET200M IM no.3. After fixing profibus connector this address is no longer exist in diagnostic buffer. 2. PIW 260 is for the seconed RFID reader which connected in the same Rack with ET200M IM no.4. and of course it is still exist in diagnostic buffer.
AttachmentDiagnose.txt (117 Downloads) |
Follow us on