10/25/2017 1:54 PM | |
Posts: 12 Rating: (0) |
Dear all, i have a project with s7 1200 ,1212c CPU and i need to connect to a PC as scada station. ladder program i made and downloaded into the plc . for scada I Selected PC Station - HMI RT 1 (WinCC RT Advanced ). after selecting and programming, am not able to communicate to cpu while during run time on the pc? any idea? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/26/2017 2:23:12 PMNew subject after splitting |
|
10/27/2017 8:50 AM | |
Joined: 8/3/2009 Last visit: 11/8/2024 Posts: 14127 Rating: (1769) |
Hello jiyojose I Think you have made a mistake in the Project or you do not hat set the right PGPC Setting on the Runtime PC. Use this FAQ to check your program/configuration: https://support.industry.siemens.com/cs/de/en/view/89852595 If you have "Softbus" in the Access Point of your HMI Connection then you could deactivate the use of Simatic Net in the PC Station. If it do not work, give us a few screenshots of your configuration. Bye Murof |
Last edited by: Murof at: 10/27/2017 8:52:40 AMLast edited by: Murof at: 10/27/2017 8:53:10 AMIf this Information really helps, you could use the Rate function |
|
Follow us on