5/10/2017 3:39 PM | |
Joined: 12/7/2015 Last visit: 1/3/2023 Posts: 2 Rating: (0) |
I have a 1511-1PN with TM2x24, but I cann't read the velocity. I connect for test button. If I set TM modul as "Position input for Motion Controll I can read position as external encoder but velocity i have 0, I don't know why. Becouse the position was increment. Second option is use as Operating with technology object with HSC, but for me dos'nt work absolutly. I have Signal type: Pulse (A) sensor type: sourcing output In OB1 "High_Speed_Counter_1".MeasuredValue is always 0. Is Anybody know how i must configure it Please Help Me. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 5/11/2017 1:25:36 PMNew subject after splitting |
|
7/19/2017 4:21 PM | |
Joined: 11/29/2011 Last visit: 10/24/2024 Posts: 1360 Rating: (232) |
Hi, Start with looking into the SIMATIC S7-1500, ET 200MP, ET 200SP Counting, measurement and position detection under chapter "3.5 Configuring the High_Speed_Counter". If you still have issues, please upload a couple of screenshot about the configuration. I hope I could help! |
- What you read here, please check with manuals and your requirements. |
|
Follow us on