12/31/2024 11:06 AM | |
Joined: 6/11/2019 Last visit: 9/13/2025 Posts: 2629 Rating:
|
Hello AutoGen, I have written a program based on your descriptions. The blocks B003 and B019 are the switch-on and switch-off points. The block B002 is used for the safety shutdown, which switches off all pumps immediately. With the block B005 you can specify a certain delay for the additional pumps if necessary. The counter B004 is intended for suppressing the second pump when the first starts and only passes on the next pulses. The rest is the logic of the pump sequencing. As there are no more precise details about the pressure sensor, I have entered some to test the circuit. You will of course have to adapt this to your circumstances I hope you can do something with it. Happy New Year and a successful 2025, Regards Ella_68 (translated with google)
AttachmentPump 1-4.zip (245 Downloads) |
Follow us on