1/22/2019 1:07 PM | |||
Joined: 10/11/2018 Last visit: 9/15/2021 Posts: 6 Rating: (0) |
Hi, I'm fairly new to this programming game, and I'm finding it very fun so far. As an automatician, this has been something that I have been missing, to fully comprehend automation systems. Now onwards to my challenge. I'm using a S7-1214C CPU, currently working on my motor controll FB. I've made a PLC data type, called HMI_Motor, that I intend to use for my faceplates in the HMI. When I add parameters, such as inputs, outputs etc for the FB, everything works when I use drag and drop from the list (cannot rember name of it) above the block interface page. But when I finnaly drag the HMI_Motor TAG into the block interface, it turns red, and gives the error "Access is invalid. User manual gives me the code 604:4542 and the following text:
I've had a look at the DB names and components, but I'm not sure what to look for in order to correct my mistake. In advance, thank you for all answers, improvment is key AttachmentMNW_HMIMotor.pdf (117 Downloads) |
||
Follow us on