11/22/2015 4:00 PM | |
Joined: 10/17/2011 Last visit: 7/19/2022 Posts: 148 Rating: (3) |
Hi, I am using PCS7 V8.1 SP1 . I used templates for MonAnl, MotL,VlvL ,PIDLean etc from APL library. Right now, I don't have AS hardware, so I used PLCSIM to test these charts. But it is found that when i go online after downloading to PLC SIM, every channel driver(digital as well as analog) gives Bad output. How to resolve it? I have configured related hardware also. But when I use similar templates in PCS7 V8.0 on another laptop , its working fine. No bad Bad value at channel driver. Why so? Please help. With Best Regards, Damayanti ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 11/23/2015 3:49:57 PMNew subject after splitting |
|
11/23/2015 11:03 AM | |
Joined: 10/26/2011 Last visit: 5/14/2024 Posts: 761 Rating: (190)
|
Hi, first, you should enable the simulation mode. Set the input SimOn to 1. If you set the SimOn=1 then the Process Value Input SimPV_In is activated (the PV_In is bypassed).
You can also use the input bytes and words from PLCSIM. |
Last edited by: Thunderstorm at: 11/25/2015 7:01:43 PMSIMATIC PCS 7 - Overview |
|
This contribution was helpful to2 thankful Users |
11/24/2015 4:42 PM | |
Joined: 10/17/2011 Last visit: 7/19/2022 Posts: 148 Rating: (3) |
Hi, I am using input bytes from PLCSIM. Still it gives bad channel status. Regards, Damayanti
|
7/14/2016 1:49 PM | |
Joined: 12/23/2011 Last visit: 11/22/2022 Posts: 143 Rating: (0) |
i'm same problem please help me thanks. |
7/14/2016 1:59 PM | |
Joined: 12/23/2011 Last visit: 11/22/2022 Posts: 143 Rating: (0) |
hi i think this block not support with plcsim |
Follow us on