1/28/2015 6:32 AM | |
Posts: 9 Rating: (0) |
Hi! I'm has just installed PCS 7 v8 SP1 with Russian localization and there is problem with alarm messages. Details: I've created project with some CFC blocks, for example MotL. By default MotL have own alarm messages which should appears in OS, for example when 3 sec has gone and there is no feedback from Motor. So, my actions. I'm downloading and compilng charts to PLCSIM. Everything is fine. Next, I'm starting compilation of entire OS with memory reset (Tags and messages are checked). Compilation successful. BUT. There is no messages in Alarm Logging regarding my MotL. So when my engine hasn't feedback only black icon "F" appears and there is no any alarm message. Log just says that: There were no messages to create There are no text libraries to create. Compilation log attached. Please help, what i'm doing wrong? AttachmentTRANSFER.zip (94 Downloads) |
1/28/2015 7:49 AM | |
Posts: 9 Rating: (0) |
no problem
AttachmentTHPOFile.zip (100 Downloads) |
1/29/2015 8:47 AM | |
Joined: 12/22/2014 Last visit: 10/7/2021 Posts: 173 Rating: (23) |
Have you run the OS Project Editor in WinCC Explorer? |
Greetings |
|
1/29/2015 9:10 AM | |
Posts: 9 Rating: (0) |
Of course, and Message configuration tab is disabled
|
Follow us on