7/6/2020 8:09 AM | |
Joined: 5/3/2017 Last visit: 5/21/2024 Posts: 673 Rating:
|
Hi Asad99, the easiest way to display an Analog Bar inside the vessel graphic is to use the standard object "Bar". In the application example Equipment Modules for SIMATIC PCS 7 using the example of the Chemical Industry at the equipment module "Level Control" you can find a configured bar to show the level of a vessel. With regards |
7/8/2020 10:19 AM | |
Joined: 5/3/2017 Last visit: 5/21/2024 Posts: 673 Rating:
|
Hi Asad99, if you want to use the "APL_BAR_VERTIC_1" from "@PCS7ElementsAPL.PDL" you have to made some small changes:
In the attachment you can find some pictures, that should help you. With regards AttachmentBarGraph.zip (128 Downloads) |
Last edited by: Heisenberg2 at: 07/08/2020 10:19:55 |
|
This contribution was helpful to
1 thankful Users |
Follow us on