5/21/2010 10:55 AM | |
Posts: 147 Rating: (34) |
Hi Check: S7-200 System Manual Chapter 14 - Using Data Logs From the aforementioned Manual: -----------SNIP----------- To use the data log feature, you must have installed an optional 64K or 256K memory cartridge in your PLC. See Appendix A for information about the memory cartridges. You must use the S7-200 Explorer to upload the contents of your data logs to your computer. -----------SNIP----------- If you have any questions, let us know. glhf |
Last edited by: Aristotelis at: 5/21/2010 10:56 AM |
|
5/21/2010 2:17 PM | |
Posts: 60 Rating: (6) |
One other option you might consider is to use S7-200 PC Access to poll for these values and store them into an excel spreadsheet. Please see this link: https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&objId=21601611&load=treecontent&lang=en&siteid=csius&aktprim=0&objaction=csview&extranet=standard&viewreg=WW |
5/24/2010 9:03 AM | |
Posts: 147 Rating: (34) |
Hi sundar in order to provide Ethernet connectivity to your S7-200 PLC you have to use module CP243 1-IT. Then you impement a connection with tho OPC server
There are FAQs that can aid you: S7-200 PC Access and other OPC clients -- Configuring and programming communication -- Programming and connecting OPC clients There's plenty of info for PC Access OPC server & Excel. Alternatively, you can always use your own program, that stores the values in a (e.g. SQL) database and produces the .csv file with anything you - or your customer - want. glhf P.S. You can always use S7-1200 that comes with Ethernet (PROFINET) by default. Again, compatible with PC Access. |
5/24/2010 10:59 AM | |
Posts: 100 Rating: (2) |
Thanks aristotelis, I attached the Bill of Material for datalogging using S7-200. Pls correct the BOM from S7-200 to S7-1200. IS PLC programming software(Microwin for S7-200 or STEP 7 Basic V10.5 for S7-1200) Must to store the real value in PC. I need the real time value in every predetermined time(without Clicking any button or Automatically)in .csv format. Regards, L.V.Sundar. AttachmentDATA LOGGING.zip (149 Downloads) |
5/25/2010 9:11 AM | |
Posts: 100 Rating: (2) |
Thanks Aristotelis, Now i attached the revised Bill of material and Architecture for data logging using S7-200 plc. If there is any modification means could u send me the reply. I am not familiar with Visual Basic. Is it easy to change the real time value to .CSV format (every predetermined time). Regards, L.V.Sundar. AttachmentData_Logging.zip (104 Downloads) |
Follow us on