8/15/2017 3:09 AM | |
Joined: 4/22/2010 Last visit: 6/5/2024 Posts: 82 Rating: (1) |
Dear Experts, I went onsite yesterday to upgrade the SE PO of the 410 CPU but found out later that online SE PO upgrade is only possible with PCS7 Version 8.1 or higher. The problem is that , they are using PCS7 V8.0 . Below are the things I've observed yesterday: 1. I’ve have tried to check the license key using my laptop and found out that there is a license inside. Im using a virtual machine with PCS7 V8.2 installed. The “connect target system” option is also available on ALM. 2. But when we used the same license key usb on their Engineering Station, we got a different response. The ES can’t see what’s inside the license key USB. The “connect target system” option is also not available on ALM Is there any work around or other solution to this issue without upgrading the system (PCS7 version upgrade)? Were planning to upgrade the SE using my laptop but I'm not sure if will still have compatibility issues since they are using a lower version of PCS7. Kindly see attached files for your reference. Hope you can help me with this. Thank you in advance. Best Regards, Boycemento AttachmentSE PO UPGRADE.zip (32 Downloads) |
8/15/2017 10:16 AM | |
Joined: 6/19/2017 Last visit: 6/12/2024 Posts: 8140 Rating: (165) |
Closed cause question posted twice.
|
My Forum is the place to personalize your profile, |
|
Follow us on