6/6/2014 4:30 PM | |
Joined: 5/18/2006 Last visit: 10/21/2020 Posts: 170 Rating: (63) |
See the attached link (links to CFC Manual for V8.0 SP4): Setting up As Wide Interconnections (CFC V8.0 SP4) Note this manual states that each OB3x is limited to 4800 Bytes for AS-Wide Interconnections. Also, notes that the volume of the interconections is CPU based ("The number of AS-wide interconnections that is permitted depends on the performance of the CPU"). The 10,000 Bytes/sec I mentioned was the orginal values published when first released. Also, note the discussion concerning the CPU setting of 30% for AS-Wide Communication. cabreytj |
This contribution was helpful to1 thankful Users |
Follow us on