9/2/2020 12:24 PM | |
Joined: 3/14/2008 Last visit: 11/11/2024 Posts: 2126 Rating: (951)
|
Hi, Did you set the BATCH launch coordinator security settings to NTLM mode or compatible mode with the correct authorizations? This way, the batch data can be read. |
If I could help you, you can use the RATE button. Thank you. |
|
9/2/2020 1:11 PM | |
Joined: 3/14/2008 Last visit: 11/11/2024 Posts: 2126 Rating: (951)
|
Are you using PLCSim? or a real CPU If PLCSim is used, you have to start Batch Control Server as interactive user and not by the launch coordinator. You need to adjust the properties of "Bfserverhostx and restart the PC: Go to Start->Run and enter: dcomcnfg, select DCOM configuration: Bfserverhostx and click on Properties in the short menu. Switch to "Identity" tab and select the "Interactive user" option. Close and restart PC. |
Last edited by: Oreca at: 09/02/2020 13:15:03If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
9/2/2020 1:13 PM | |
Joined: 12/6/2019 Last visit: 10/20/2024 Posts: 6 Rating: (0) |
I am using PLCSIM |
9/3/2020 11:09 PM | |
Joined: 3/14/2008 Last visit: 11/11/2024 Posts: 2126 Rating: (951)
|
Hmm Ok, Can you upload the installed software just to be sure? Maybe some component is missing...Did you install a package or did you install the software components by yourself? If you don't know is also an answer. Did it work before? Maybe you can check the steps in the following manual: Batch V8.0 Getting Started Start around page 51 with the OS compile+download and continue from there... |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on