6/7/2018 2:14 PM | |
Joined: 6/19/2008 Last visit: 6/1/2023 Posts: 46 Rating:
|
Hi Guys, I have a silly problem to book back PO Licences. According to manual it should be done like this:
Using the Options > Charts > Book back process objects menu command, you can deregister the process objects of a program that you no longer want to run on the CPU by returning these objects to the Automation License Manager. The program is thereby deleted from the CPU.
------------------------------------------------------------------------------------------ |
Last edited by: Kargan at: 6/7/2018 2:14:34 PMLast edited by: Jen_Moderator at: 6/7/2018 2:43:46 PMNew subject after splitting |
|
6/7/2018 2:28 PM | |
Joined: 3/14/2008 Last visit: 8/3/2024 Posts: 2079 Rating:
|
Hi Kargan, Maybe your are in the wrong view. Go to Component View and set the cursor at the Charts folder of the CPU you want to book back PO. Go to Options->Charts and select Book Back Process Objects. Did it succeed |
If I could help you, you can use the RATE button. Thank you. |
|
6/7/2018 2:53 PM | |
Joined: 6/19/2008 Last visit: 6/1/2023 Posts: 46 Rating:
|
You are my Man Oreca !!! Thx a lot - it works. It's interesting why this is not described in manual more... precisely |
6/7/2018 3:08 PM | |
Joined: 3/14/2008 Last visit: 8/3/2024 Posts: 2079 Rating:
|
Thanks! Yeah, it can be very confusing. The same goes for updating your SFC block types from the master library. You need to be on the Charts in the master library in order to update. It can be described a lot better I agree... |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on