2/22/2020 7:44 PM | |
Joined: 5/6/2010 Last visit: 6/2/2024 Posts: 1966 Rating: (274) |
Hello HBCM_, which PLC do you want to use? This is important for any suggestion. regards |
2/25/2020 4:49 AM | |
Joined: 10/7/2005 Last visit: 6/6/2024 Posts: 3008 Rating: (1051) |
It seems to be saying -31663 based on HBCM_'s screendump. That then would be 8451(hex) as the error code which - as per HTA Instruction help - means "Non-supported data type in the OUT parameter". Can't argue with that one as a DWORD is used by HBCM_ for the OUT parameter whereas the HTA help insists that "You can reference the following data types using the pointer in the OUT parameter (ASCII): STRING, WSTRING, Array of CHAR, Array of WCHAR, Array of BYTE, Array of WORD" |
Cheers |
|
This contribution was helpful to1 thankful Users |
2/26/2020 6:52 AM |
|
Joined: 10/25/2019 Last visit: 5/20/2024 Posts: 278 Rating: (20) |
one more who doesn't read posts completely. |
Follow us on