2/17/2009 12:11 PM | |
Posts: 1776 Rating: (95)
|
Hi, you have different possibilities: - use OPC communication to get data from PC |
2/17/2009 12:48 PM | |
Posts: 1776 Rating: (95)
|
Hi, for OPC see WinCC online help for communication dito. |
2/17/2009 4:20 PM | |
Joined: 4/5/2006 Last visit: 4/24/2024 Posts: 917 Rating: (63) |
Hi razoh, you have to create a new "OPC channel" in WinCC explorer "Tag managment" on your PCS7 project (make sure DCOMM are correctly configured!!! look under www.opcfoundation.org--> Download --> White Papers) The both station has to be configured in same workgroup and need same user/password configured. OPC server has to be in runtime, if not OPC client (PCS7 project cannot see tag on your panel pc). Continue with configuration described in manua April gave you. Very strange you cannot comunicate directly between PCS7 and S7-300, maybe something wrong in coniguration you made, or maximum connection nr reached (look into S7-300 diagnostic for that). Direct connection between PCS7 and S7-300 is the best way to get information (just create a new connection manually in WinCC explorer "Tag managment -> Simatic Protocol Suite -> TCP/IP" Regards |
2/18/2009 4:54 AM | |
Posts: 2661 Rating: (279)
|
Hi razoh, As CBo & April have suggested, I would recommend using the Ethernet communication tosend data (using DB)from S7-300to S7-400 for WinCC tag generation... See if the following thread helps: Communication between PCS7 AS and 315CPU's via Ethernet |
5/7/2018 6:46 AM | |
Joined: 6/19/2017 Last visit: 4/26/2024 Posts: 7957 Rating: (162) |
New question published by AutoGen_7870139 is split to a separate thread with the subject Establish the communication between PCS7 AS (v9.0) and 314CPU (s7 v5.3). Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on