5/10/2021 7:12 AM | |
Posts: 198 Rating: (60) |
Hello, There could be multiple reasons for this error message: Have you checked your SIMATIC shell (go to "This PC" in Finder and click the SIMATIC Shell folder). From there, I right clicked the SIMATIC shell to go to properties. Please check if you have selected the network adapter selection is correct, and then hit ok (do not use encryption or migration mode). It will work as long as you then can see both the engineering station and OS Server setups below in the left pane. There is a detailed explanation for using SIMATIC Shell for the terminal bus configuration: FAQ Link If this is fine, please check the following:
The other possibilities could be related to access rights too - Please refer this FAQ and check if the following conditions are also addressed - FAQ Hope this helps |
Last edited by: TechnoBlaze at: 05/10/2021 07:14:00Last edited by: Jen_Moderator at: 05/10/2021 13:58:00Optimized links. |
|
This contribution was helpful to2 thankful Users |
5/11/2021 5:08 AM | |
Joined: 8/20/2016 Last visit: 3/4/2024 Posts: 81 Rating: (0) |
Hello TechnoBlaze I do as your instruction and I see every is right, but I am beginner at PCS7, you can see the pictures about my system in following link, may be you can see anything problem. [snip] Best regard. Attachmentpicture.zip (218 Downloads) |
Last edited by: Jen_Moderator at: 05/11/2021 07:23:54Removed link and added file as an attachment. |
|
5/11/2021 6:32 AM | |
Posts: 198 Rating: (60) |
Hello, Select 'Full Control' as well in the folder's advanced sharing properties' permissions. Does it work now? |
5/11/2021 10:40 AM | |
Joined: 8/20/2016 Last visit: 3/4/2024 Posts: 81 Rating: (0) |
Hello I already checked but I do not see any abnormal, address in Simantic Shell and network connection is the same. |
Follow us on