12/19/2014 7:13 AM | |
Joined: 3/14/2008 Last visit: 5/7/2024 Posts: 2066 Rating: (928) |
Could it be that it is a Setting CPU to test is because the CFC program is different from the online. Should be no issue if you still want to monitor parameters... |
Last edited by: Oreca at: 12/20/2014 8:00 PMIf I could help you, you can use the RATE button. Thank you. |
|
12/20/2014 7:59 PM | |
Joined: 3/14/2008 Last visit: 5/7/2024 Posts: 2066 Rating: (928) |
Hello Microman, Sorry, I saw an error in my comment... I meant if it is a function (FC) that your trying to monitor instead of a function block (FB). But strange that is works well under sim...What attributes do you have set for this input your trying to monitor? |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on