9/16/2010 11:08 AM | |
Posts: 86 Rating:
|
Are you changing in module drivers? if yes, they are generated and will be generated again. Yer |
9/23/2010 11:08 AM | |
Posts: 96 Rating:
|
Hiwolf08, The CFC is meant to automatically save all the changes you make. The only think that will cause this is if you are working in a auto generated CFC (used for driver blocks) or F blocks (safety matrix blocked, generated whenever you compile your safety marix) or if you update the process tag type. If this is not the case then can you please confirm which runtime group it is adding the blocks (the runtime group can be found out by clicking on the green box on the block) Hope this was helpful. If this does not help then please send some screen shots. regards, Minhaj
|
9/23/2010 8:47 PM | |
Posts: 14 Rating:
|
hi minhajie, the one you are referring to is not my case, im not working with automatically generated cfc, and due to the nature of the problem is not possible to take a screenshot, i will try to explain itand i know its not suppose to happen because theres i no SAVE or UNDO in PCS7: i insert an OR block an rename it then i insert an AND block and rename it,the momenti try to connect the output of an already existing block (anyone) to the OR block a message appears "the block doesnt exist" and then both blocks dissapear (OR & AND blocks) like if i never did anything at all. This can happen after i did a lot of changes so is kind of frustrating. im receiving one message error continuosly that perhaps has something to do with the problem, i add a screenshot. any idea? Regards |
9/24/2010 9:24 AM | |
Posts: 86 Rating:
|
Hi, an old remidy is to reorginaze the project, because the references will be checked and repaired if possible File > save as > with reorginaze (slow) Yer |
9/24/2010 12:05 PM | |
Posts: 96 Rating:
|
Hiwolf08, If you don't want to do what Yer said then I would recommend you to close all application and do a system restart and then try one more time. It is a common practise but I though it is worth mentioning in case you haven'tdone it? regards, Minhajie
|
10/5/2010 1:07 PM | |
Joined: 11/15/2006 Last visit: 5/7/2021 Posts: 1319 Rating:
|
Is there a second user editing the chart or are you the only one who is working on this project? |
Have Fun! |
|
Follow us on