5/17/2016 11:34 AM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927)
|
Hi Stephane, Please check the following link. I think the answer is listed in there. Regards |
If I could help you, you can use the RATE button. Thank you. |
|
5/18/2016 8:26 AM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927)
|
Good morning Stephane8, I see what you mean. The project was created on a computer which was set in Windows Language settings as Dutch. Once the project is created, it's not possible to change the language...I believe... The only way is to create a new project under the correct language and transfer everything. Do you have also problems opening the project? Otherwise, you have to set the option under properties of the project: "Can be opened under any Windows language settings". |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
5/18/2016 9:16 AM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927)
|
Hi, Thx for the feedback! Well, I could imagine that seeing a different language in your multiproject is not very "nice". If there are any problems: Opening the project under a different language is not successful, than you can use the option I gave you in my previous post. |
If I could help you, you can use the RATE button. Thank you. |
|
5/18/2016 2:07 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927)
|
Hi Mark, Does that work for sure? I saw a post from Wizard, but it did not work like that..but this was a long time ago.. https://support.industry.siemens.com/tf/ww/en/posts/s7-project-language/3219/?page=0&pageSize=10 |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on