8/22/2020 1:44 AM | |
Joined: 8/1/2019 Last visit: 11/6/2024 Posts: 300 Rating: (3) |
Can Simatic Batch receive commands from a higher level system to eventually pass it to SFCs? |
8/22/2020 5:28 AM | |
Joined: 9/9/2015 Last visit: 10/28/2024 Posts: 728 Rating: (280) |
From Simatic Batch to CFC, you have the param blocks to get the variable. Then from the CFC level, you can use the param you get from the batch , transfer to SFC instance or SFC type (input). Now it depends on what "high-level system" you have, to communicate with Simatic Batch and do the order creation. Without detail study yet, what I think it is possible to be realized. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
Follow us on