5/20/2013 12:52 PM | |
Joined: 8/31/2010 Last visit: 4/29/2024 Posts: 1509 Rating: (222) |
Hello MrBin, I'm not aware if the said application has a native driver for S7-1200 which supports sybolic addressing. (I fear if such thing is available, as even WinCC v7.2 doesn't have one). Otherwise you can onfigure a OPC server to pull out data from S7-1200 and then use the process values at your end. Have a look at How do you connect a PC station to an S7-1200 with OPC? Hope this helps. |
Like it? Rate it! |
|
5/22/2013 10:51 AM | |
Posts: 90 Rating: (0) |
Thanks Ganes10! I will read that document. I can use that OPC with Intouch? |
Follow us on