2/19/2017 8:34 AM | |
Posts: 88 Rating: (4) |
Dear all, How to communicate Sentence PAC 3100 with ET 200 SP module by modbus protocol..Please help by giving sample program. Regards Afeef
|
2/19/2017 9:15 AM | |
Joined: 2/6/2015 Last visit: 9/8/2024 Posts: 61 Rating: (19) |
Dear Afeef, You haven't told us if you are using TIA Portal or Simatic Manger. Kindly be specific while requesting Samples as there are many compatibility/upgradation issues that we are facing with siemens. However, for your assistance I have collected a few links that will be helpful for you: Here is a sample which might be useful, if you are using TIA V12/13: <Master Slave Communication via a CM PtP using the Modbus RTU Protocol> Hardware related information will be available here: I hope it will be helpful for you Regards |
Kaushal Kumar Joshi |
|
This contribution was helpful to1 thankful Users |
2/19/2017 11:53 AM | |
Posts: 88 Rating: (4) |
Dear Kuashal Using tia portal,please help with neccesary documents and program if possible. Regards Afeef |
2/20/2017 10:19 AM | |
Posts: 88 Rating: (4) |
modbus rtu |
2/20/2017 10:57 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1054) |
hi afeef, there are several FAQ and application samples that could help you: Master Slave Communication via a CM PtP using the Modbus RTU Protocol there are some more FAQ and application sample available. you find them by using the search window in the upper right on this page. hope this helps, regards, |
FCK WAR! |
|
This contribution was helpful to1 thankful Users |
Follow us on