11/27/2012 2:56 PM | |
Posts: 378 Rating:
|
Hello chriswam, I guess the problem could be the driver for USB adapter, Try this steps: 1. Unplug your USB adapter. 2. Uninstall MicroWin. 3. Restart your PC. 4. Plug your USB adapter. 5. Install USB adapter driver (from the CD comes with USB adapter) then unplug and plug the USB adapter now your pc should detect automatically and check on device manager. 6. Install MicroWin. 7. Go to control pannel (from your Windows 7 Ultimate) and open Set PC/PG Interface then you can set PC Adapter or Serial cable 9. Open Microwin and check on the communication tab and see if your problem solved. NB: When you install all the softwares, right click and Run as Administrator. Hope helps! |
This contribution was helpful to
1 thankful Users |
11/28/2012 11:29 AM | |
Posts: 378 Rating:
|
Hi You can download the driver from here: http://support.automation.siemens.com/WW/view/en/21226394 For more see this link: http://support.automation.siemens.com/WW/view/en/37855423 Regards |
Follow us on