4/3/2007 8:49 AM | |
Posts: 66 Rating: (0) |
Hello I am ussing a CP 343-1 lean (module version: V 2.0.16) The lean is connected to a CPU312 I want to use the web browser so I can acces the lean whit internet explorer But this doesn't work. I hope someone can help me. thank Timmermans See attachement. (Step 7 archive) AttachmentTest_inb.zip (526 Downloads) |
4/3/2007 11:41 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (318)
|
Dear Timmermans, You may find the information for the update in the next FAQ: Firmware Update V2.0 for SIMATIC NET CP 343-1 Lean (6GK7343-1CX10-0XE0)please download also the new GSDML file! With the update, the CP 343-1 Lean (order no. 6GK7343-1CX10-0XE0) is functionally compatible with the predecessor version. It can therefore be configured with the same STEP 7 / NCM version. If only the compatible functions are used, it is not necessary to upgrade STEP7 or NCM. To be able to configure the new functions of the CP 343-1 Lean (6GK7343-1CX10-0XE0) you require version V5.4 SP1 + Hotfix 2 with Hardware Support Package HSP 1014, or alternatively Step7 V5.4 SP2and NCMS7 for Industrial Ethernet. NCMS7 is fully integrated in the STEP7 environment. For HSP1014 see Hardware Support Packages (HSPs) |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on