1/9/2017 10:31 AM | |
Posts: 111 Rating: (15) |
Hello,
==> Found some information about the operation system: both are compatible with WindowsXP. I couldn't found other information about the compatibility. WinAC 416-2 PCI: https://cache.industry.siemens.com/dl/files/750/1169750/att_37393/v1/ACcont_e.pdf PCS7 BOX RTX: https://mall.industry.siemens.com/mall/en/us/Catalog/Product/6ES76504AA000AA0
==> There is no information aobut this configuration/ application available. Is it possible to try it? Windows XP should be working. I hope this might help you. |
This contribution was helpful to1 thankful Users |
1/9/2017 3:19 PM | |
Posts: 111 Rating: (15) |
1) There is a new Software for the diagnose: See here: https://support.industry.siemens.com/cs/ww/en/view/29237745 The new software you can get here: https://support.industry.siemens.com/cs/ww/en/view/29316343 2) Can you see the card in the hardware manager? Is there perhaps also a driver problem of the PCI bus? |
This contribution was helpful to1 thankful Users |
1/9/2017 4:19 PM | |
Posts: 4 Rating: (0) |
Thanks, 1) Is it neccessary to use this software? 2) No, I have no problem with driver. Maybe another reasons? |
1/11/2017 8:39 AM | |
Posts: 111 Rating: (15) |
Hello, I have no other ideas from my point of view. If a reinstallation of the SW packages doesn't help, perhaps the PCI card is incompatible, in fact? Perhaps you open a Support request and the technical support may help you: https://support.industry.siemens.com/My/ww/en/requests I read a little bit the manual of the PC Box RTX, and as far as I understand, the WinAC is running directly in the PC, so it is possible to run the automation directly in the PC Box (with the correct licences). See here: https://support.industry.siemens.com/cs/attachments/106127254/ps7box_b_en-US.pdf?download=true (page 16) ==> My question: Isn't it possible to transfer the automation from the CPU 416-2 PCI card to the PC BOX WinAC? |
Last edited by: Min_Moderator at: 1/11/2017 12:52:44 PMEdit link to permanent one |
|
Follow us on