3/31/2017 7:41 PM | |
Joined: 12/18/2014 Last visit: 4/27/2024 Posts: 32895 Rating: (4066)
|
To 1.) So it is. Download via LSC loads only the last CSV file. To 2.) This is also correct. It saves only 50 CSV files to the SD card. Each file contains a maximum of 20,000 line entries. To 3.) There must be a pause of 500 ms between each log operation. If the time is not reached, the system will not be logged. The appendix contains an extract from the current manual. AttachmentLOGO! 8 Soft manual 0BA8 2016_07 (FS4) pages 273+274.pdf (66 Downloads) |
This contribution was helpful to1 thankful Users |
4/1/2017 4:16 AM | |
Joined: 12/18/2014 Last visit: 4/27/2024 Posts: 32895 Rating: (4066)
|
No. There's no way. |
This contribution was helpful to1 thankful Users |
Follow us on