11/22/2024 5:24 AM | |
Joined: 8/20/2024 Last visit: 1/8/2025 Posts: 1 Rating:
|
I have an ET200eco PN communications module with eight IO-Link ports that can be repurposed as digital I/O (6ES7148-6JJ00-0BB0). I have setup six ports as an IO-Link 2I + PQI port and have setup the appropriate configuration for the IO-Link device in S7-PCT The documentation associated with the module mentions that ports configured with IO-Link could use the otherwise unused Pin 2 on each of the ports as a DIQ, but there is scant detail on how to do this; and there is no explicit option to setup the DIQ pin WITH the IO-Link port options provided in TIA Portal. Ref to document: https://support.industry.siemens.com/cs/ww/de/view/109816068 The particular part of the manual that describes the use of a DIQ pin alongside an IO-Link port is in Section 4.1: Is there something that I'm missing here, or is there a mistake in the manual and that we've made a bad assumption here. Any help in clearing up any misunderstanding would be of great help. Regards, Craig Sacco |
Last edited by: Moderator_Lan at: 11/22/2024 08:17:47link optimized |
|
Follow us on