4/16/2016 11:59 PM | |
Joined: 11/29/2011 Last visit: 10/24/2024 Posts: 1360 Rating: (232) |
Hi, Have you try to disconnect the other 2 ports? The upload procedure is detailed in SIMATIC Programming with STEP 7 V5.5 under chapter "19.3.1 Uploading a Station". |
Last edited by: MicroMan at: 4/17/2016 12:03:18 AM- What you read here, please check with manuals and your requirements. |
|
4/17/2016 12:04 AM | |
Posts: 6 Rating: (1) |
No,i did not disconnect any of the other ports. all the system nodes is already viewed,but i could not connect to any of them. |
4/17/2016 12:07 AM | |
Posts: 6 Rating: (1) |
i have this manual and i do the steps as explained;but no response. |
4/17/2016 12:12 AM | |
Joined: 11/29/2011 Last visit: 10/24/2024 Posts: 1360 Rating: (232) |
Hi, What I have in mind is the Communication Resource limitation of the CPU. See What is the maximum number of OPs that a CPU S7-300 can communicate with? I never seen this problem before but please keep us in the loop! |
- What you read here, please check with manuals and your requirements. |
|
4/17/2016 2:06 AM | |
Joined: 5/28/2008 Last visit: 11/6/2024 Posts: 4516 Rating: (839) |
Hello, Please tell us the setting of Set PC/PG interface and also tell us the address of your CPU. I ask these questions as these should be an error in assigning addresses which will trigger the error you showed in the screen shot "33:16656" Please see the followings: How can you set up the online connection again between the PG and the CPU?STEP7 Error Messages |
Ayman Elotaify |
|
4/17/2016 8:34 AM | |
Joined: 5/28/2008 Last visit: 11/6/2024 Posts: 4516 Rating: (839) |
Hello, There are another way to test Profinet network using the free software PRONETA PRONETAPRONETA 2.3.0.26 Commissioning and Diagnostics Tool for PROFINET |
Ayman Elotaify |
|
This contribution was helpful to1 thankful Users |
4/17/2016 4:31 PM |
|
Joined: 10/10/2010 Last visit: 10/25/2024 Posts: 307 Rating: (15) |
try to set hardware configuration carfully |
Follow us on