10/16/2015 4:32 PM | |
Joined: 3/14/2015 Last visit: 6/20/2024 Posts: 93 Rating:
|
Hi, I have a bigger problem. I have a 416-3dp as the main controller and a 315-2dp as the local controller.these CPUs are not even in the same multiproject and it's not possible integrate the projects. Now I have exchage data between two cpus via 342-5 for 315 and IF for 416.I don't know how.It's an urgent. Can mr hosseini and other friends help me please? I'm really in trouble ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 10/19/2015 12:03:55 PMNew subject after splitting |
|
10/16/2015 8:25 PM | |
Joined: 3/14/2015 Last visit: 6/20/2024 Posts: 93 Rating:
|
I have done this type of connection for ethernet but does it work for profibus?? |
10/19/2015 12:34 PM | |
Joined: 8/25/2005 Last visit: 7/5/2024 Posts: 1161 Rating:
|
Hello Hasan1987, There is an example: How do you program communication blocks FB14 "GET" and FB15 "PUT" for data exchange in the S7 program of an S7-300 CPU? You have to modify it a little bit but I hope it will be helpful! Good luck |
Follow us on