10/7/2024 7:49 AM | |
Joined: 8/3/2009 Last visit: 11/5/2024 Posts: 14087 Rating: (1766) |
Hello braaay which FW Version do you use in your S71500 and which Image Version do you have on your Panel? (then we can say more about settings...) If you want to simulate you have to check the PGPC Interface settings -> if you hae set the AccessPoint S7ONLINE in your HMI connection settings in the HMI project then you have to set this Access Point to the Networkcard.TCPIP.1 (if you wan to communication to a real PLC) or to PLCSim if you do also a PLc simulation on the same system. (check also this FAQ) Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on