11/28/2009 7:01 PM | |
Posts: 3 Rating:
|
:( no answer :( |
12/23/2009 3:09 PM | |
Posts: 510 Rating:
|
The attribute S7_m_c = true just moves the item to the Tag database in WinCC. It does not create the message. The alarm blocks in Step 7 can be used to create the messages. The following link is for WinCC Flexible but it will give you an introduction to the some of the alarm blocks. http://support.automation.siemens.com/WW/view/en/24013249. here is a link for WinCC http://support.automation.siemens.com/WW/view/en/23730649 Also you might consider implementing Report System Error. This automatically creates hardware and software errors associated with the PLC. These are configured in the Hardware config. the online help is very good for this. I hope you will find this helpful. Regards, billwest |
Follow us on